IMPORTANT SAFETY RECALL

Surge Protection Devices Manufactured Before 2003

Some surge protection devices can overheat under abnormal electrical conditions, posing a possible fire risk to persons and property


8 Series Surge Strip


7 Series Surge Strip

How do I know if I have a recalled unit?

1. Look for bar code label on bottom of surge strip

2. Confirm that the Model Number is included in table below, AND

3. The two numbers that follow the first letter(s) in the serial number sequence indicate year of manufacture. The unit is included in the recall if the numbers are 93, 94, 95, 96, 97, 98, 99, 00, 01,or 02

Frequently Asked Questions

Affected Model Numbers

8 Series 7 Series
NET8 NET7
NET8N NET7T
NET7T-C PER7
PER8T PER7C
PER8TR PER7T
PER8TR-CN PER7T-CO
PER8TVR PER7T-U
PER8XTV PER7TX137
PRF8T2 PER7-U
PRF8TT PER7X148
PRO8 PRF7
PRO8T2 PRF7T
PRO8T2C PRO7
PRO8T2MP12 PRO7C
PRO8T2MP12B PRO7T
  PRO8TV
  PRO7TX183

 

Stop using surge strip if you have one of the recalled products

Have an affected product?

Submit a claim